10/14/2016 3:42 PM | |
Joined: 8/3/2009 Last visit: 7/11/2024 Posts: 13284 Rating:
|
Hello Prasanna It depends on the Trigger. If you use a Script or a Systemfunction for writing in a Internal Tag then the Event Value change will not be executed. See the following FAQ: https://support.industry.siemens.com/cs/de/en/view/57132412 Chapter 1 But if you use a IE Field for example it will be executed. And yes of course you can set Internal Tags out of a Script without no problems. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on