10/4/2013 3:08 PM | |
Posts: 58 Rating:
|
if i use a udt as inout variable. my datamemory for the 300 compiled in TIA portal is way higher. with the 1500 i don;t got this problem. what's the diffrent between the plc's that caused this problem? |
Last edited by: O_Moderator at: 10/9/2013 9:29 AMnew subject after splitting from /tf/WW/en/Posts/97394#top |
|
10/5/2013 2:05 PM | |
Joined: 10/7/2005 Last visit: 2/17/2025 Posts: 3036 Rating:
|
Hello v.kerstholt it seems that Siemens has changed the way complex Block parameters (e.g. Structures, UDT etc.) are accessed inside an FC/FB for the 1500 (I haven't tried so myself yet, soI take your word and that of the FAQ for it). Doing so in a 300 or 400 will certainly increase the memory requirements (and runtime) of the FC/FB consderably as you already observedand you can find the reasons for this in the thread Shall UDT make the difference in CPU Scan Time? I hope this helps |
Cheers |
|
This contribution was helpful to
1 thankful Users |
10/9/2013 2:51 PM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello, using optimized data storage you can run your programs on the S7-1200/1500 at optimum performance. In this way you achieve a cycle time that is shorter on average by a factor of 3. See the FAQ in the internet in refer to the differents between standard and optimized block access: http://support.automation.siemens.com/WW/view/de/67655611 With best regards |
10/11/2013 9:55 AM | |
Posts: 58 Rating:
|
Cicero, i know that. it's the fact I'm investigatingif it is usefull to migrate with as7-300 to tia portal. With best regards, Vincent |
10/30/2013 3:38 PM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello, see the different of UDT/S7-PLC data tpye between STEP 7 V5.5 and STEP 7 (TIA Poral) V12 in the FAQ: http://support.automation.siemens.com/WW/view/de/67582844 With best regards |
Follow us on