1/13/2024 1:01 PM | |
Joined: 1/13/2024 Last visit: 4/23/2024 Posts: 10 Rating: (0) |
Hello friends The work memory cpu 1200 1214 is about 98% full. If I use an external memory, will it decrease the work memory? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/15/2024 11:37:28New subject after splitting |
|
1/15/2024 6:56 AM | |
Joined: 3/11/2019 Last visit: 7/9/2024 Posts: 1511 Rating: (270) |
Hi, there is no external "work memory". Only the "load memory" can be extended due to the use of an SIMATIC Memory Card. The only thing you can check, is the used firmware version of your CPU. Firmware V4.6 for S7-1200 available"Firmware V4.6 is able to provide more memory for all CPUs because of code customizations. CPU modules of the HW generation V4 (article number: 6ES721x-1xx40-0XB0) already in use can use this extension through the firmware update. In addition, the SNMP service is disabled by default. regards sancruz |
Last edited by: sancruz at: 01/15/2024 07:01:02Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
1/31/2024 5:37 AM | |
Joined: 1/13/2024 Last visit: 4/23/2024 Posts: 10 Rating: (0) |
I upgraded the firmware to 4.6, about 30% was added, thank you very much |
1/31/2024 5:39 AM | |
Joined: 1/13/2024 Last visit: 4/23/2024 Posts: 10 Rating: (0) |
It helped a lot and decreased by about 5%. tnx |
This contribution was helpful to1 thankful Users |
Follow us on