8/3/2017 2:13 PM | |
Joined: 10/11/2006 Last visit: 4/19/2024 Posts: 5820 Rating: (787)
|
Hello, please note, that the motor temperature signal is included in the encoder cable! And 1FT7, 1FK7 and most other motors are of course equipped with temperature sensors. For details about different thermal models, have a look in the function manual S120 in chapter 9.5. Also note, that KTY84 was discontinued by the manufacturer and the motors are changed to Pt1000 sensors. |
Last edited by: TechTeam at: 8/3/2017 2:15:37 PMWith best regards, |
|
8/3/2017 3:28 PM | |
Joined: 6/28/2017 Last visit: 12/20/2022 Posts: 661 Rating: (39) |
It doesn't matter KTY84 or Pt1000, I still can't find its ends around motor. the CU320's X522 terminals are empty. Looks weirdly! The encoder cable goes straight to X202 bypassing X522 which is used for temperature sensors.
Read about that cable (6fx8002-2dc20-1ag0). Found nothing there regarding two wires for T.sensor included or whatever. Please point me in that string at specifications. I'm still having doubts about presence of KTY84 or PT1000 inside of servo-motor (1FT7...). P.S. Chapter 9.5 states that if encoder cable connected, the Drive can take all relevant data of motor from EEPROM which is situated on encoder PB. That's clear! But where is written list of that data? Whether the current temperature of winding is included? Cheers |
Last edited by: Msorich at: 8/3/2017 3:47:16 PM |
|
Follow us on