7/29/2010 3:24 PM | |
Joined: 4/23/2007 Last visit: 12/11/2023 Posts: 75 Rating: (8) |
What do you want to do? Do you want to write a function, i.e. a c-script with an if query? |
Runis |
|
7/29/2010 3:39 PM | |
Posts: 27 Rating: (0) |
for example if a<4 then b=b+4 where must I write it and how can I show b at IO field ?? |
7/30/2010 1:48 PM | |
Posts: 27 Rating: (0) |
your said thing is not exist. I have no sample project. if I have it, I can solve. in other scada programs (citect) I can do but dont wincc. |
8/3/2010 7:52 AM | |
Posts: 27 Rating: (0) |
I did but there are some errors, I can not undestand. can you send me picture of program page in wincc?? |
8/3/2010 8:37 AM | |
Posts: 19 Rating: (1) |
Hi, mailahmet! Sending you a picture with example of C-script containing if...else. You can find script in button properties -> events -> mouse -> click. AttachmentGraCS.zip (1307 Downloads) |
Last edited by: Username at: 8/3/2010 8:38 AM |
|
8/5/2010 8:42 AM | |
Posts: 27 Rating: (0) |
thanks username, your program is good. but it depend on the button. I want, it must independ anything. can you do it ?? |
Follow us on