3/7/2019 7:31 PM | |
Joined: 10/5/2015 Last visit: 2/10/2022 Posts: 2 Rating: (0) |
I have a similar application from this thread: PLC, HMI, and RS232C., except with a 1500S software controller running on a IPC427E. I have 12 scales. If I use a the Moxa unit, one for each scale, how can I address the unit in the 1500S? Each Moxa unit would go to a Scalance switch. Since this is a 1500S application I would also consider reading from the devices directly into Windows and sharing the data with the 1500S via OPC, is this a viable option? This seems more difficult. Thanks for any help with this. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/8/2019 6:44:55 AMNew subject after splitting Last edited by: MTI_jdpeeno at: 3/8/2019 1:24:12 PM |
|
Follow us on