2/15/2017 1:02 PM | |
Posts: 648 Rating: (95) |
Dear Harshal7, it is possible. Look at this example application:https://support.industry.siemens.com/cs/ww/en/view/50708061 First check the compatibility of PCS7 and WinCC. Use the Compatibility tool:https://support.industry.siemens.com/cs/ww/en/view/64847781 With best regards rh1990 |
2/16/2017 6:29 AM | |
Posts: 21 Rating: (5) |
Dear rh1990, Thanks for your reply, of course I checked that page already. I just need the link from where I can Download actual Industry Library for WinCC comfort It seems it is not a freebie & easily available on web |
2/16/2017 6:35 AM | |
Posts: 21 Rating: (5) |
Also, WinCC Comfort (TIA Portal ) V13 SP1 Upd1 is compatible with PCS7 V8.1 Regards, Harshal |
Follow us on