2/3/2010 1:09 AM | |
Joined: 10/7/2005 Last visit: 10/6/2024 Posts: 3024 Rating: (1054)
|
Hello Raednabeel While I haven't done so myself yet with the 154-8 PN/DP CPU, it surely will have to possible. Have a look at chapter 3.2 of itsmanual (which you can download rom HERE)and you'll see that you have plenty of communciation options. Please note that the 154-8 PN/DP CPU belongs to the S7-300 family which means that you must use the FB's (NOT SFB's) for any S7-communications that you program in it (i.e. GET/PUT, BSEND/BRCV and/or USEND/URCV). In your 400 you will however have to use the correspondingSFB's. I hope this helps |
Cheers |
|
2/3/2010 10:39 AM | |
Posts: 96 Rating: (7) |
Dear fritz, Thank you for your post it was helpful, the answer was in the manual you have directed me to it at pages 29 & 30 Belong side this , it will be found in Communication with simatic manual at 2.5.14 BR رائد نبيل حماد |
This contribution was helpful to1 thankful Users |
Follow us on