5/5/2015 2:53 PM | |
Posts: 14 Rating: (0) |
I add another SS (Sorry I was unable to add another on the same original topic message) |
5/6/2015 6:40 PM | |
Posts: 14 Rating: (0) |
Hi I did the compare procedure with the PLC and the SINAMICS integrated, the PLC has everything equal, the SINAMICS has differences at the Loading Parameters section. After running a Detailed comparison Scout told me this: Detailed comparison (IDEXA:14919) No relevant differences Differences have only been determined in the decimal places that are not displayed or in access level 5 parameters and are therefore not displayed. I'm sorry but I'm still a little bit new to this software, how do I run something like that with the IM-155-5 to see where's that issue, in the Diagnostics windows of the Interface Module says Diagnostic Status: Unknown. I upload the results of the SINAMICS comparison. Thank you *Edit I was checking with a CPU 1500 and I found the Compare Online/Offline option, with the d425-2 that option is not enabled on the TIA Portal. Only on the Scout. AttachmentSIMOTION SCOUT document.pdf (137 Downloads) |
Last edited by: Engbakerymach at: 5/6/2015 11:54:40 PM |
|
Follow us on