1/18/2021 10:30 AM | |
Joined: 11/29/2011 Last visit: 7/17/2024 Posts: 1358 Rating:
|
Hi, Try to go online with the configuration. See if the diagnostic suggest something obvious. If you save the diagnostic buffer an upload it to the topic, we can have a look at it. Without knowing your application / See the diagnostic buffer: Check if the End Resistors Profibus plugs set correctly Check if The "Server module" installed securely on the Remote IO station Check if the backplane is secure Check the configured modules are matching the configuration, and installed securely into the backplane. See the manual under diagnostic: SIMATIC ET 200SP interface module IM 155-6 PN/2 HF
|
- What you read here, please check with manuals and your requirements. |
|
1/24/2021 10:28 AM | |
Joined: 4/9/2020 Last visit: 4/10/2024 Posts: 2 Rating:
|
Hi, Thanks You very much. There was a profibus cables problem. Kind regards |
Follow us on