Industry Online Support
Technical Forum
10/12/2009 1:25 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Dear Pouya_PCS, Beside IM360 or IM361, there are a max of 8 cards allowed. So when you have 20 cards you will have three racks. A digital card most are 40mm. But there are card who are 80mm. You need two cables 368. You can connect one IM361 to IM360. The other IM361 can be connected to first IM361. See manual: http://support.automation.siemens.com/WW/view/en/8859629 See chapter 8. Best regards, Wizard |
Follow us on