1/27/2014 10:44 AM | |
Joined: 6/29/2011 Last visit: 6/7/2024 Posts: 127 Rating:
|
Hi Pittiplatsch. i have 3 no;s of im151-8 cpu modul number of 6ES7151-8AB01-0AB0 ok.And 1 PC for SCADA Wincc Flex 2008 SP.2 here i attached my system layout. AttachmentIM151.pdf (84 Downloads) |
param |
|
2/3/2014 8:36 AM | |
Joined: 6/29/2011 Last visit: 6/7/2024 Posts: 127 Rating:
|
Hi, Can i get any Example configuration Program for that .please help
|
param |
|
2/3/2014 9:02 AM | |
Posts: 1368 Rating:
|
Hello tkm, the configuration of a PROFINET communication is very simple: ==> create a TIA project and insert a new device. Choose ET200S-> IM 151-8 ==> repeat this twice ==> go to the net view. One IM151-8 is IO-Controller, the other must be IO-Device. ==> To change the operating mode to "IO-Device", click on the ethernet interface of the module. In the properties -> operating mode choose "IO-Device" and assign it to the Port of the IO-Controller. ==>The modules are connected automatically. ==> The last step is to assign the profinet name to the io-devices.This can be donevia "online&diagnostic" More information you find in the PROFINET manual http://support.automation.siemens.com/WW/view/de/19292127 Greetings, Pittiplatsch |
2/3/2014 1:49 PM | |
Joined: 6/29/2011 Last visit: 6/7/2024 Posts: 127 Rating:
|
hi here i attached program backup pls check i did correct network config ,if i did mistake pls correct me and thank u for helping me
AttachmentWipro_fat.zip (106 Downloads) |
param |
|
2/3/2014 2:06 PM | |
Posts: 1368 Rating:
|
Hello tkm, can you make a screenhot? thx |
2/4/2014 4:36 PM | |
Joined: 6/29/2011 Last visit: 6/7/2024 Posts: 127 Rating:
|
Here i attached
AttachmentScreen shot.zip (147 Downloads) |
param |
|
Follow us on