9/30/2011 12:21 PM | |
Posts: 2348 Rating:
|
IM151-8 generally very similar to 314 - as far as i know even CPU inside is the same. But i didn't really understood your question |
9/30/2011 5:20 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello, For more information on IM 151-8 cpu, pl read this Manual. |
VANDE MATARAM..... |
|
10/1/2011 9:26 AM | |
Joined: 6/29/2011 Last visit: 6/7/2024 Posts: 127 Rating:
|
Hello, For more information on IM 151-8 cpu, pl read this Manual. manual have some virtual error leave it. please tell me et200s is required for im151-8 cpu or not |
param |
|
10/4/2011 10:51 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Dear suvarn, The IM151-8 CPU is a header module of ET200S, with integrated CPU. You do not need another CPU. Have you seen this Thread: /tf/WW/en/Posts/33504 Here it's explained how to configure IM151-8 CPU in Simatic Manager. If you want to communicate with TP177-B using Profibus, you need a Profibus Master module next to IM151-8 CPU. What conditions do you have to comply with when configuring ET 200S modules? Best regards, Wizard |
10/4/2011 10:54 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Dear paranthaman, The IM151-8 CPU is a Header for ET200S, with integrated CPU. (When you want to use IM151-8 CPU, you need ET200S module for inputs/outputs) What conditions do you have to comply with when configuring ET 200S modules? Best regards, Wizard |
Follow us on