Industry Online Support
Technical Forum
9/17/2012 1:51 AM | |
Posts: 108 Rating: (2) |
Hi, I am trying to enable the web server of an IM151-8 V3.2 PN/DP CPU using Step7 V11 + SP2 + Upd4 in TIA Portal. Although the web server works, it does not work fully. Parts of the web server are unavailable, including the following: Module information, topology, variable tables and customer pages. In fact, the web server seems tobehave as if there were no memory card inserted, even though there is. Refer to the following section of the user manual for information on this: IM151-8 web server. Ihave tried the same configuration with two different CPUs and it has not worked with either. Refer to the attached screenshots to see how the web server has been configured in TIA Portal. Thanks in advance for your help! Jason AttachmentScreenshots.zip (59 Downloads) |
Last edited by: jasonr at: 9/17/2012 2:08 AM |
|
Follow us on