4/20/2016 11:27 AM | |
Joined: 3/27/2012 Last visit: 7/22/2024 Posts: 179 Rating: (4) |
Hi, I already changed IM308 and then changed the Flash Memory for the config (used Com Profibus to download config) and still the same. I attach the project 3357@@st.s5d. Function FX115 is where we see the error code 0x019D that copied by Secure FB58 to SW3610 for Mixer 5 (At the begining of the problem was Mixer 7 and the same code 0x019D was written to SW3614). By Profi Trace shows the Node is OK !!! AttachmentReimelt - 09-02-2016.zip (155 Downloads) |
Last edited by: AhooraJafari at: 4/20/2016 11:34:30 AM |
|
Follow us on