10/25/2013 11:20 AM | |
Joined: 11/23/2011 Last visit: 6/25/2024 Posts: 202 Rating: (32)
|
Hello GuiMauri, very useful for establishing a connection between LOGO! and S7-1200 is the example you already send. I attach the whole link with the zip-file, where also example projects are included, for other people to see: http://www.automation.siemens.com/salesmaterial-as/software/applications/logo/s7-1200_communication.zip When more than one LOGO! devices are connected and you have also an S7 communication partner in the application, you have to ensure that the network properties (including also the PC)are set right. In this case maybe the documentation of this application example with it's explanations will help your for this and give you an approach to solution: http://support.automation.siemens.com/WW/view/en/68585346 When you have other questions don't hesitate to ask. Greetings, KM_AS |
This contribution was helpful to1 thankful Users |
Follow us on