12/17/2023 1:26 PM | |
Joined: 5/8/2010 Last visit: 9/10/2024 Posts: 19 Rating:
|
Hello everyone, I’ve created a small project using Wincc Unified PC, and I want to generate reports from archived data. The Excel report is successfully connected to the Wincc Unified server, and data is visible without any issues. However, when I tried to import the template at runtime, it doesn’t get added. I attempted to resolve this by uninstalling and rienstalling the software, but the problem persists. On another computer with the same installation, everything works fine, but on the computer where l’m currently working, importing the template is impossible. l’m stuck and awaiting your help. The attached photo shows the problem. |
12/22/2023 8:01 AM | |
Joined: 8/3/2009 Last visit: 3/13/2025 Posts: 14990 Rating:
|
Hello redha05 Which Version of WincC Unified and Office do you use exactly? you should not use a *.xls file use a *.xlsx instead (in your screenshot there is an old xls file selected) Bye Murof |
If this Information really helps, you could use the Rate function |
|