9/6/2021 6:03 AM | |
Joined: 3/27/2019 Last visit: 1/27/2022 Posts: 6 Rating:
|
After a problem with drive cliq cable it is impossible to perform the calibration. The code is same, program was not changed. Please help, why it happens? Thats what we found (pic. 1). DB708.DBW20 should be in range between 7000 and 7002. Then it will be possible to call FC610 - Acycle write. Inside FC610 calling of SFC58 (pic. 2). And the return value of this SFC is the condition to be able to call it (DB708.DBW20). In help of SFC58 we found information (pic. 3) that we need to taking action. In our case DB708.DBW20 has value -32587 (80b5 in hex). And homing cannot be done. Is it right that we have to change value of this ret_value? Because this FC does not calling anymore because of wrong value in DB? ------------------------------------------------------------------------------------------ |
Last edited by: Famous_94 at: 09/06/2021 07:03:35Last edited by: Famous_94 at: 09/06/2021 07:18:35Last edited by: Famous_94 at: 09/06/2021 07:19:33Last edited by: Jen_Moderator at: 09/07/2021 05:55:32New subject after splitting |
|
9/6/2021 7:08 AM | |
Joined: 3/27/2019 Last visit: 1/27/2022 Posts: 6 Rating:
|
Sorry for additional post, but i can't load 3 images simultaneously Pic. 2 |
9/6/2021 7:09 AM | |
Joined: 3/27/2019 Last visit: 1/27/2022 Posts: 6 Rating:
|
Pic. 3 |
Follow us on