6/5/2024 9:00 PM | |
Joined: 8/26/2015 Last visit: 7/13/2024 Posts: 1 Rating: (0) |
Dear seyed, Have you a screenshot of the Automation License Manager before you use the upgrade license? I mean a Screenshot of ALM whe the license was still V6.X If yes, Could you share it please? I have the problem that in the ALM some components of PCS 7 in the family column show SIMATIC STEP 7 instead of SIMATIC PCS 7 and I'm not sure if a Software Upgrade package license AS/OS Engineering license will upgrade all the old licenses. If any one have an idea about it, I will be very grateful. Original version: PCS 7 V7.1 SP3 >> Target version: PCS 7 V9.1 ------------------------------------------------------------------------------------------ |
Last edited by: jairogaliciamexico at: 06/05/2024 21:04:36Last edited by: Jen_Moderator at: 06/06/2024 06:54:19New subject after splitting |
|
Follow us on