8/4/2017 3:04 PM | |
Joined: 6/22/2017 Last visit: 11/27/2023 Posts: 12 Rating: (0) |
Hello there, In this block ocurred error of" There is a time stamp conflict with at least one block" . Call and end_call are red How to fix this? Call BLD 3 = L 5.0 CDB OPN DI 15 TAR2 LD 1 A "SEQ00_OFF_SEQ" = DIX 0.0 A "SEQ00_INIT_SEQ" = DIX 0.1 LAR2 P#DBX 0.0 UC "FB_00_Automatico" LAR2 LD 1 L DIW 6 T "SEQ00_StepNumber" CDB BLD 4 End Call A "SEQ00_Ativo" R "SEQ00_INIT_SEQ" A "Est00_ModoManual" R "SEQ00_Ativo" A "SEQ00_Ativo" AN "HOME_Ativo_00" = "Est00_Habilita_Vis_Auto" ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/7/2017 10:12:28 AMNew subject after splitting |
|
Follow us on