6/9/2011 9:21 AM | |
Posts: 487 Rating:
|
Hi very basic IN = Input , OUT = Output IN/OUT Flag or merker |
6/9/2011 9:25 AM | |
Joined: 10/7/2005 Last visit: 9/28/2023 Posts: 2988 Rating:
|
Hello safety4ever I know its painful and wish I could tell you otherwise, but the one and only correct thing to do is to change the FC call Parameters to make sure they comply with the following: IN: Read only access inside FC OUT: Write only access inside FC. MUST be written to every time FC is called IN_OUT: Read/write acccess None of the above rules existed for S5 FB's and IN or OUTdeclaration forthem was of pure "cosmetic" nature. Since the S5-S7 converter doesn't take any of the above rules intointo account, it is unfortunately your job to do so now. |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on