10/15/2019 6:47 PM | |
Joined: 10/24/2012 Last visit: 3/8/2024 Posts: 307 Rating: (21) |
Dear Experts, I am facing this problem and i don't know how to cater this issue. I made a OPC UA connection with 1217C CPU.Before doing the station configuration and importing xdb file in station configuration manager i added 2 DBs in my program compile the program and download it to the CPU after that compile the configured PC station which generated the xdb file then i import that file in my station configuration manager and successfully run it and i have connected the OPC UA server to my PLC S7-1217C. I tested it and it worked fine. Now i did a lil changing in my PLC program in which i added a new DB in my PLC program and download it to the PLC and its working fine as you can see in the picture but in OPC SCOUT UA server view i can only see 2 DBs in my system,as you can see in the attached pictures, the 3rd DB is not displaying in the SYM table. Is it compulsory to always reconfigure the station configuration manager, whenever i need to do any modification in my PLC program? Thanks in advance. Kashir Saeed. ------------------------------------------------------------------------------------------ AttachmentPictures.zip (38 Downloads) |
Last edited by: Jen_Moderator at: 10/16/2019 05:50:41New subject after splitting Kashir Saeed. |
|
10/16/2019 5:04 PM | |
Joined: 7/7/2010 Last visit: 4/30/2024 Posts: 14655 Rating: (2349)
|
Are you trying to see the newly added DB using the original station configuration? Good luck with that.
|
science guy |
|
Follow us on