11/20/2018 12:48 PM | |
Posts: 11 Rating: (0) |
Hi, am using ET200SP and CM PTP module for Modbus rtu communication with the device. 1st I configured Modbus comm load & it is getting done bit from there. but in the Modbus master its showing an error 81E2 and busy. my Modbus register starts from 0000. so should I use it as 40001 is this correct, because the register 0000 is 16bit register. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/20/2018 2:35:05 PMNew subject after splitting |
|
11/20/2018 1:14 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819)
|
Hello, if this is Holding register, then yes... |
With best regards... |
|
Follow us on