9/24/2015 6:37 AM | |
Posts: 9 Rating:
|
dear sir i am commissioning g120 using 6SL3310-1TE32-6ABx vector module with brakeing resister. motor rated frequency is 50hz but due to production customer is requested to run in 63hz ,so i change p1082 and p2000, while running in 63hz dc voltage increase upto 840v then drive trip due to fault f30002, my question is can i run motor in 63hz ,if its can then which parameter want change,plz best regards mani ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/24/2015 10:41:10 AMNew subject after splitting |
|
9/28/2015 3:30 PM | |
Joined: 10/11/2006 Last visit: 7/26/2024 Posts: 5880 Rating:
|
Hello, it seems your parameter setup for the motor is not correct and the braking chopper does not work. We would recommend to contact the customer support: Support Request : http://www.siemens.com/automation/support-request |
With best regards, |
|
Follow us on