12/6/2019 5:53 AM | |
Posts: 33 Rating: (0) |
I have 6 digital outputs. initially i want to move 0 in each DO. I want to get step output. for example, initially i have D0,D1....,D5=0, after delay of 1 second i want to make it D0=1 and D2,D3,D4,D5=0. like that i want to use those digital outputs as an array and increment it. please help me if you have a solution in LADDER. In short, i want to increment an array of 6 bit by for 1 each second ------------------------------------------------------------------------------------------ |
Last edited by: Vishaljp at: 12/06/2019 05:54:27Last edited by: Vishaljp at: 12/06/2019 06:00:32Last edited by: The Helping Hand at: 12/09/2019 16:43:15New subject after splitting |
|
12/9/2019 4:43 PM | |
Joined: 8/21/2014 Last visit: 4/26/2024 Posts: 949 Rating: (13) |
Please don't post questions twice -> closed. Please use: Increment of an array of 6 boolean by 1 |
My Forum is the place to personalize your profile, |
|
Follow us on