9/7/2022 2:52 PM | |
Joined: 5/20/2021 Last visit: 3/19/2024 Posts: 7 Rating: (0) |
The error is at the attachment. I try to connect with chrome to the IP address. I setup the IEM IP based, with DHCP, I create a NAT network to connect the IEM. And in the option during the installation that says Obtain hostname with DHCP I choose no. Here I read some post that is similar I think. similar error. |
Follow us on