Industry Online Support
Technical Forum
3/23/2010 12:35 AM | |
Joined: 10/7/2005 Last visit: 9/12/2024 Posts: 3020 Rating: (1054)
|
Hello klps there is no generic "one size fits all' programming guide since the various S5 CPU's differ in funtionality and supported command set from each other. Every CPU has as such its own programming guide which contains the info that you are after and a good place to start downloading these is from the link below: S5 CPU's Programming manuals Another really good source are the Hans Berger books who wrote a few books on the subject of S5 (again, CPU/System dependent). Should you need to do some "hardcore" S5 editing, these Books are worthwhile trying to get (google "Hans Berger& S5" and see if and where these are still available) I hope this helps |
Cheers |
|
Follow us on