10/29/2009 5:35 AM | |
Joined: 10/7/2005 Last visit: 11/6/2024 Posts: 3026 Rating: (1055) |
Hello Valli your consultant means IEC-60870-5-103 and your answer to him will have to be: "No it does NOT, the communciation between the PLC and Simocodes follows Profibus Standards, of which the most important ones are":
IEC 60870-5 is the "main" standardand predomanitely used in Substations (DNP3 is very similar to it should you know DNP3), wheras the "103" is the additional so called"Companion standard for the informative interface of protection equipment" |
Cheers |
|
This contribution was helpful to1 thankful Users |
8/24/2014 10:44 PM | |
Joined: 9/1/2005 Last visit: 11/6/2024 Posts: 4109 Rating: (195) |
new question published by RaviSis split to a seperate thread with the subjectCan the Siemens PLC support IEC60870-5-103. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on