3/14/2016 2:31 PM | |
Posts: 17 Rating: (0) |
Hello everyone, I have been trying to configure Information Server 2014 for a couple of days and I cant do it. According to the manual, the installation and configuration should be very simple. Anyway, I am having the following errors (i am attaching pictures to explain myself better): Picture 1: Installed software Picture 2: Installed licenses Picture 3: note that the Information Server does not seems to recognize the licenses installed Picture 4: note the "database not ready yet" message. What does it mean? Picture 5: when i select my project and click "add", the message "project container not found on the temp data" appears. What does it mean? If anyone knows something that may help me, that would be great. Thanks! AttachmentInformation Server Configuration Problem.zip (520 Downloads) |
3/17/2016 4:35 PM | |
Posts: 648 Rating: (95) |
Hi fpecc, did you change your computername after the installation? With best Regards rh1990 |
3/18/2016 12:30 PM | |
Posts: 17 Rating: (0) |
Hi rh1990, No, i didnt. My Pc name is "PM-PC". Maybe there is a problem with the "-"? Best regards, fpecc |
3/18/2016 1:00 PM | |
Posts: 17 Rating: (0) |
I will try that, thank you |
5/4/2016 11:59 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by AutoGen_5632859 is split to a separate thread with the subject PCS 7 Information Server failure "IS failure on not existing subscription". Best regards |
8/1/2016 3:15 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by lucifer123 is split to a separate thread with the subject Configure Information Server 2014 Update 1. Best regards |
This contribution was helpful to1 thankful Users |
1/26/2017 3:54 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by PaulArg is split to a separate thread with the subject Information Server problem, Error after login. Best regards |
Follow us on