1/9/2019 7:34 AM | |
Joined: 4/28/2015 Last visit: 2/2/2023 Posts: 3088 Rating:
|
Hi, no. The IOT2000 itself runs the Linux OS. Of course you can use another PC with Windows to establish a SSH connection to the IOT2000 or to write programs for it. There are lots of examples about connecting the IOT2000 to a cloud. The engineering of the programs is mostly done on a PC running Windows, the execution on the IOT2000 running Linux. I hope things are bit more clear now Best regards! |
This contribution was helpful to
1 thankful Users |
2/2/2023 7:08 AM | |
Joined: 4/28/2015 Last visit: 2/2/2023 Posts: 3088 Rating:
|
Hi, this repository represents the BSP as well as the Example Image (extended BSP with software, functionality, etc.) for both devices - IOT2020 and IOT2040. Best regards! |
Follow us on