11/17/2020 4:51 PM | |
Joined: 3/16/2020 Last visit: 9/12/2024 Posts: 13 Rating: (0) |
Hello, I have a Client Server application configured in WinCC v7.5 upd 4. When I activate the Run Time in the Client it gives me a permanent dialog box that says that the initial image is not configured, in the server the initial image is configured in clients, but the dialog box persists and I can't see the images in run time, please if you can help me, thanks
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/18/2020 09:32:04New subject after splitting Last edited by: Jen_Moderator at: 11/18/2020 09:43:50Edited text for better reading. |
|
11/18/2020 4:33 PM | |
Joined: 9/27/2006 Last visit: 9/13/2024 Posts: 12282 Rating: (2683) |
Hello Yusiel; What you are trying to do is called a "WinCC-Client without project", where all the configuration, including screens, are located only in the server. Maybe the application example in the following link can be useful to you: Configuration of a Client–Server System with WinCC V7.5 https://support.industry.siemens.com/cs/ww/en/view/109771695 Hope this helps, Daniel Chartier |
11/18/2020 4:59 PM | |
Joined: 3/16/2020 Last visit: 9/12/2024 Posts: 13 Rating: (0) |
Thank you very much Daniel I hope this link can help me, greetings |
11/25/2020 1:36 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello Yusiel, maybe, the Windows-User from the Client-PC has not see FAQ: https://support.industry.siemens.com/cs/ww/en/view/868014 part 3. Operating system
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
6/3/2021 6:46 PM | |
Joined: 3/16/2020 Last visit: 9/12/2024 Posts: 13 Rating: (0) |
|
Follow us on