3/23/2010 12:44 AM | |
Joined: 10/7/2005 Last visit: 6/8/2024 Posts: 3008 Rating: (1051)
|
Hello WIAG possibly because you have only a single "1" in the initial value column. Useeither: - "64 (1)" (if all array elements are to have the same initial value of "1") OR - "1,2,3,4,5,6,7" (up to 64values, each seperated by a comma, this allows you to have different initial values per array Element) I hope this helps |
Cheers |
|
This contribution was helpful to3 thankful Users |
3/23/2010 2:19 PM | |
Posts: 3 Rating: (0) |
That's perfect... thank you very much. |
This contribution was helpful to1 thankful Users |
Follow us on