3/6/2020 1:10 AM | |
Joined: 3/1/2018 Last visit: 7/30/2023 Posts: 8 Rating: (0) |
Hi All. I am trying to find a solution to a problem of: "Inputs or outputs are used that do not exist in the configured hardware" (see attachment) I know this problem was explored before but I could not find anything that will help me to resolve the issue mentioned above. I believe the problem began when I was trying to us SCL as a function with the FOR loop to capture pulses from my encoder via High-Speed Counter which also caused an error on CPU. Because that was only the experiment to see if I can do it (I am not experienced with SCL ). To eliminate the main error on the CPU I simply deleted the FB and all data blocks attached to it. That fixed the CPU error but the warning is still there when downloading to the device and "GO TO" option is sending me to the assignment list (see attachment) where I don't see anything to indicate the issue as all the memory tags associated with the SCL are removed and only tags left are the ones that were absolutely fine. I would be grateful if anybody could share some possible solution as this is driving me crazy. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/06/2020 07:20:56New subject after splitting |
|
Follow us on