3/19/2008 12:38 AM | |
Posts: 2661 Rating: (279) |
Sorry, I did not make myself clear enough. The first option I suggested was to insert a Windows folder in Windows Explorer in to your project and store your documents in this folder (see attachment). Tip: When you insert special characters before the folder name, the folder moves to the top most position and is easy to locate. The second option (of inserting documents from within the Step7 project) is only possible with PCS7. You cannot insert documents in native Step7. Installing DOCPRO will make no difference. AttachmentDokument1.pdf (157 Downloads) |
Follow us on