3/25/2016 5:00 PM | |
Posts: 2 Rating: (0) |
i've installed my TIA Portal V13 on my E: drive without any problem. Then i've tryed to install the update Sp1 Upd4 using the TIA portal Updater software. But the updater software doesn't allow me to select other drive than C: ?! My D: & E: are proposed but 'Required' (Benötigt) & 'Temp' (Temporär) memory are not verified (=0). see picture joint... Is there a fix for this ? Thx
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/29/2016 3:02:46 PMNew subject after splitting |
|
3/29/2016 3:37 PM | |
Joined: 8/31/2013 Last visit: 5/26/2024 Posts: 607 Rating: (41) |
That is means your C Driver does not has the enough space of your installation |
Warm Regards |
|
7/12/2017 12:40 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
New question published by uzi18 is split to a separate thread with the subject After Installation: SP1 updater force me to install update on C:. Best regards |
Follow us on