10/20/2022 8:14 AM | |
Joined: 5/30/2022 Last visit: 9/24/2024 Posts: 582 Rating: (96) |
Hi AutoGen_3394064, The LOGO! modules must be connected to the CPU, so installation in 2 racks is not possible. You would need to use 2 LOGO!, one slave of the other, I attach information about it: Changing LOGO! to master/slave mode |
If this information really helps, you could use the Rate function. |
|
Follow us on