10/9/2023 9:13 AM | |
Joined: 9/24/2021 Last visit: 9/30/2024 Posts: 3 Rating: (0) |
Hi all, I just installed Hotfix 3 STEP 7 V5.7 SP1 and now my Simatic Manager doesn't start anymore. I get to see the splash screen, which dissipates after a while and then nothing happens. What can i do to troubleshoot/fix this issue? Attached is part of my Windows Event log Maik Attachmentevent.zip (302 Downloads) |
Last edited by: maikverheijen_ict at: 10/09/2023 09:42:34 |
|
10/9/2023 9:38 AM | |
Joined: 9/24/2021 Last visit: 9/30/2024 Posts: 3 Rating: (0) |
Attached is the error message from the Windows Event log |
Last edited by: maikverheijen_ict at: 10/09/2023 09:41:00 |
|
10/9/2023 11:35 AM | |
Joined: 9/24/2021 Last visit: 9/30/2024 Posts: 3 Rating: (0) |
Did the repair installation but unfortunately it did not help |
Follow us on