12/11/2023 8:17 AM | |
Joined: 12/20/2016 Last visit: 6/16/2024 Posts: 42 Rating: (0) |
Hi Interlogis, Is it for s7 1200/1500 or s7 300/400? I use s7 300. So, some instruction and datatype are not support. How can i use for s7 300? Thanks, Khang. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/11/2023 12:22:36New subject after splitting |
|
12/11/2023 3:03 PM | |
Joined: 8/12/2021 Last visit: 7/12/2024 Posts: 321 Rating: (29) |
Hi! ThisFAQdiscusses the functions that can be used with respect to each range of the PLC for variables of type DATE_AND_TIME. |
Last edited by: The Helping Hand at: 12/11/2023 15:04:55Text formatting optimized If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on