6/4/2012 9:20 PM | |
Joined: 7/19/2010 Last visit: 7/3/2024 Posts: 50 Rating:
|
Hi Dear, I have a problem, I´m trying convert a step5 program to step7, but there are instructions that no convert: See: // L RS 34; // *** Error in Line 3841 (FB 200): Invalid operator. *** +I // LIR 0; // *** Error in Line 3844 (FB 200): Command not defined. *** // TIR 2; // *** Error in Line 3874 (FB 200): Command not defined. *** // T BS 255; // *** Error in Line 3920 (FB 200): Invalid operator. *** // DO BS 255; // *** Error in Line 3922 (FB 200): Command not defined. *** Is there any manual with these instructions? The program is attached. Thanks!!! AttachmentPROGRAST.zip (264 Downloads) |
Esdras Lopes Cardoso |
|
7/3/2019 8:22 PM | |
Posts: 3 Rating:
|
Hi Esdras, how did you fix the problem with the BS operator? |
Follow us on