Industry Online Support
Technical Forum
12/8/2012 11:58 PM | |
Joined: 9/27/2006 Last visit: 12/20/2024 Posts: 12307 Rating: (2695) |
Hello Kamran; There is no compatible interface module for the S5-100U, unfortunately. Not from Siemens, nor from Phoenix Contacts. Here are some documents that will show this: Problem: You have an old S5 system Interface modules adapter 6EZ2 for Simatic S7-300 and S7-400 Data Sheet DB EN S5/S7 ADAPTER - Phoenix Contact Hope this helps, |
12/10/2012 4:50 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, i would use a 6ES5 318-8MB12 or 6ES5 318-8MB13 and connect it via profibus with the new CPU. If you need this part - i have few of them. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster withinnovative PLC-Tools |
12/12/2012 4:49 PM | |
Joined: 9/27/2006 Last visit: 12/20/2024 Posts: 12307 Rating: (2695) |
Hello Kamran; These documents and links should help you out: Siemens Product support for the IM 318B: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=6ES53188MB13&caller=view ET 200U manual: ET 200U Distributed I/O Station Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/12/2012 4:50 PM |
|
Follow us on