1/20/2020 12:14 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear vishal p., I faced this problem before. The issue might relate to server data. If you try to configure a server-client configuration / single OS configuration, it will work. Did you assign OS Server in your Client OS and download to the Target Station? Please also check these two links. Interlock button remains greyed out CEMAT V8.2 Faceplate Issue - Can't access Interlocks and Groups |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
1/20/2020 12:58 PM | |
Joined: 3/13/2014 Last visit: 5/2/2024 Posts: 44 Rating: (1) |
Hi JazTai Thanks for your response , I already configure station OS configuration Check in attachment.
|
1/20/2020 1:10 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear vishal, So now you are operating at "Pm3-OS1" this station and the button is still disabled? A screenshot on this station faceplate will be good. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
1/20/2020 2:06 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Can you do the following 1. a full OS Compilation 2. then reassign the OS Server data for OS Client, and 3. do a OS Client download again?
|
Please give me 5 stars Rating if my post is helpful for you. :) |
|
1/22/2020 2:21 PM | |
Joined: 3/13/2014 Last visit: 5/2/2024 Posts: 44 Rating: (1) |
Hi Expert, Please help me to solve this problem. Thanks in advance.. |
Follow us on