3/25/2009 12:10 PM | |
Joined: 4/24/2006 Last visit: 10/14/2024 Posts: 8745 Rating: (1168) |
Dear Tariq, Well, in that case it is probably better to Uninstall WinCC flexible and reinstall it. Perhaps this link, might help: http://support.automation.siemens.com/WW/view/en/28465761 Best regards, Wizard |
3/26/2009 9:11 AM | |
Joined: 4/24/2006 Last visit: 10/14/2024 Posts: 8745 Rating: (1168) |
Dear Tariq, What is the exact version of WinCC flexible? (including any Hotfixes) Best regards, Wizard |
3/26/2009 9:21 AM | |
Joined: 7/28/2007 Last visit: 5/15/2024 Posts: 50 Rating: (1) |
Dear Wizard, Its version is VERSION: 2007 Build: V1.2.0.0_1.55.0.1 Regards, |
3/26/2009 9:31 AM | |
Joined: 4/24/2006 Last visit: 10/14/2024 Posts: 8745 Rating: (1168) |
Dear Tariq, Here is a link, where you can download Hotfix 4 for WinCC flexible 2007: http://support.automation.siemens.com/WW/view/en/28882233 Please install and look if problem is still there. Best regards, Wizard |
3/26/2009 10:05 AM | |
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating: (77) |
Hi You can try to use thefunction "Save and Optimze" in the menu bar of "project". Maybe this will help you. Bye |
Follow us on