Industry Online Support
Technical Forum
5/10/2013 11:21 AM | |
Joined: 4/8/2010 Last visit: 1/16/2024 Posts: 89 Rating: (0) |
This interrup call ? OB40 ? |
5/10/2013 1:01 PM | |
Joined: 9/27/2006 Last visit: 5/26/2024 Posts: 12257 Rating: (2668)
|
Hello Umbi; Yes the hardware interrupt usedfor end-of-cycle functions (comparators) with the SM 355is OB40. See sections 3,4 and 5.2 of this manual for more details: SIMATIC S7-300 SM 335 - High-speed analog mixed module for SIMATIC S7-300 You can find more information and links on hardware interrupt processing in the following FAQ: What is a hardware interrupt and how do they work in the S7-300 system? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/10/2013 1:05 PM |
|
5/10/2013 2:14 PM | |
Joined: 4/8/2010 Last visit: 1/16/2024 Posts: 89 Rating: (0) |
Yes .. Thank-you very much .. |
5/10/2013 2:22 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi Umbi, Yes it is just that, also because the CPU 314-2DP there is just that. |
Follow us on