Industry Online Support
Technical Forum
9/28/2010 3:17 PM | |
Posts: 10 Rating:
|
Hi CGR013, You have touse the actual PLC or you can use theWinLC RTXas CPU in theHardware configuration for testing. You have to configure your PC as WinLC by using Station Configurator (Simatic net). Then you can force the tag values in WinLC and view the changes in Intouch. |
9/28/2010 3:25 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
Dear RameshK_Cimac..., You way is another possible way to simulate Intouch. I didn't try with Intouch 8.0 but with 9, 9.5 and 10 simulation works pretty good. Take a look at /tf/WW/en/Posts/42660 Hope you will find answer of your problem. Best regards, Hristo Mihalev |
9/28/2010 4:16 PM | |
Posts: 27 Rating:
|
thnks anyway. |
9/29/2010 8:19 AM | |
Posts: 10 Rating:
|
Dear UMENCHO, The reason why I mentioned to use WinLC for program simulationis thatthe PC running Step7 to be configured in Simaticnet station configurator for Intouch softwaretobrowse the tags. I faced problem when tried to simulate with PLCSIM to Intouch. Then I used WinLC configuration and successfully simulated the tags from WinLC and viewed the changes in Intouch. I have read the link provided by you. In that also the problem was not solved as per the last post from drozerce (Hi Hristo, still nothing. Here in attach I'm sending you the list with port from command promt (this is ok, I think In the next mail I'll send to you a screen shot of alarm page that I made from my application. You can see that the alarms are shown and for the database says:Connected (This says that my Dasserver configuration is ok). Is there anywhere else where I can see some reports, why I cann't make connection? |
Last edited by: RameshK_Cimacindia at: 9/29/2010 9:28 AM |
|
10/4/2010 9:26 AM | |
Posts: 10 Rating:
|
Hi CGR013, Pls find the attachment for WinLC configuration screen shots. AttachmentHw_config.pdf (507 Downloads) |
Follow us on