2/13/2024 8:23 AM | |
Joined: 11/29/2018 Last visit: 8/7/2024 Posts: 10 Rating: (1) |
I have the same problem, no matter if I compile changes only or rebuild the whole project, I randomly get "Invalid ARRAY tag" errors (Message 619:12). There is no useful solution in Help. My array is very simple: aruSamples [0.."CONST"] of "UDT". The shocking thing is that the previous variable is build up similarly aruIncoming [0.."CONST"] of "UDT" and does not return error at compile The solution is to: Rename "aruSamples" to "aruSamples1" > Compile (no errors returned) > Rename "aruSamples1" to "aruSamples" > Compile (no errors returned). It's very annoying to do this every time. Siemens should either provide real solution in the Help file or remove whatever test/rule is causing this at compile. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 02/16/2024 08:03:22New subject after splitting Please Thank & Rate if you find my post helpful. |
|
2/15/2024 10:16 AM | |
Joined: 3/11/2019 Last visit: 8/8/2024 Posts: 1550 Rating: (279)
|
Hi, should be update 5 for V17. The workaround (rename) is still necessary for the affected arrays once, but after update 5 this message should not appear anymore for new tags/arrays. At least this was the response from the technical support due to a support request. And i did not get this message in my own projects afterwards, so this should be correct. In the meantime, update 7 is available. Updates for STEP 7 V17, S7-PLCSIM V17 and WinCC V17regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |
Follow us on