6/20/2017 4:11 AM | |
Joined: 7/20/2015 Last visit: 5/20/2024 Posts: 153 Rating: (27) |
Dear All My step-7 backup have some internal error, when i reorganize (slow) this backup i am getting some error. I attach internal error & reorganize slow error snapshoot. Please help how can i resolve this erroe Software detail 1- STEP -7 V5.5=sp4 2.-WINCC 7.2+UPD-13 3- CFC 7.1+SP3+UPD1 AttachmentREOGANIZE ERROR.pdf (54 Downloads) |
Regards |
|
6/20/2017 5:19 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Sandeep Bakoliya, Compile all charts individually. Set compiler properties as per requirements. Then perform Reorganize-'slow'. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
6/20/2017 9:03 AM | |
Joined: 7/9/2015 Last visit: 5/17/2024 Posts: 3833 Rating: (557) |
Hi, please have a look at the following FAQ - hope this helps: What can you do to avoid the message "Invalid file position" (1739:10) when saving your project with "Save as ..." and the option "Reorganization (slow)"?Regards, Towome |
|
|
Follow us on