9/25/2023 10:22 AM | |
Joined: 12/23/2020 Last visit: 5/7/2024 Posts: 2 Rating: (0) |
Hello, I have two different inverters, a micromaster 440 and a sinamics g120 that control two compressors and would like, after of acceleration ramp, that each Hz of gain or delay takes 1 second if it's possible. Thanks
|
9/27/2023 2:05 PM | |
Joined: 3/27/2008 Last visit: 1/19/2025 Posts: 1157 Rating: (142) |
I may be misunderstanding this?? but can this be set by the ‘ramp’ time adjustment?? Tractor |
Tractor |
|
9/29/2023 5:01 AM | |
Joined: 3/25/2008 Last visit: 1/21/2025 Posts: 202 Rating: (8) |
Hello what kind of compressor are they? do they have any management?
|
10/13/2023 9:18 AM | |
Joined: 12/23/2020 Last visit: 5/7/2024 Posts: 2 Rating: (0) |
Hello, First I apologise for error but are not a compressor but a delta blower aerzen of 200kw They are controller by PLC with setpoint fix or PID, we liked when we use the PID, each Hz of gain or delay takes 1 second after of acceleration ramp. Thank you |
10/15/2023 3:47 PM | |
Joined: 3/27/2008 Last visit: 1/19/2025 Posts: 1157 Rating: (142) |
Using the PI controller within the drive, this change you are referring to is a dynamic due to the performance of the system. If the PI controlling, and working, the rate of control required can only be managed empirically. As I look at my response it sounds like an excuse, but these things do take some time to set up, with a PC connected and using STARTER, sat on a packing crate trying to understand what is working or not? I have attached a drawing which may help, it refers to G120C for a Stairwell Pressurisation control system, but the parameters still apply to MM440 or MM430, and G120C. I hope this is a help with getting the response you require. Tractor
AttachmentG120C PID control.pptx (491 Downloads) |
Tractor |
|
This contribution was helpful to1 thankful Users |
Follow us on