10/24/2017 5:05 AM | |
Posts: 4 Rating:
|
Hi everyone I'm having problems with some GSD devices. An intermittent fault sends some devices to failure for a few seconds. These devices are always 'GSD Device' type, and have the option 'Use IEC V2.2 LLDP Mode' selected by default, with no possibility to deselect it. Siemens IO devices have this option deselected. I have tried to select it on each device and on the CPU but the system reacts the same. I attach a document where you can see better. Thanks in advance. Errors: Diagnostics buffer of the module PLC_CPU [CPU 1513-1 PN] Article no. / name Component Version 6ES7 513-1AL01-0AB0 Hardware 2 - - - Firmware V 2.1.0 Firmware expansion Firmware expansion --- Rack: 0 Slot: 1 Serial number: S C-H8KW16762016 1 of 529; Event ID: 16# 02:39CB Error: IO device failure - chd_vfd_5 Outgoing event Event type: OK 10/19/2017 7:17:14.234 PM (Coding: 16# 34 00 00 05 14 EE FB F0 30 2B 88 98 39 CB 00 00 38 CB 00 00 00 00 02 20 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) 2 of 529; Event ID: 16# 02:39CB Error: IO device failure - chd_vfd_4 Outgoing event Event type: OK 10/19/2017 7:17:11.742 PM (Coding: 16# 34 00 00 05 14 EE FB EF 9B 9C 57 7E 39 CB 00 00 38 CB 00 00 00 00 02 19 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) 3 of 529; Event ID: 16# 02:39CB Error: IO device failure - chd_vfd_3 Outgoing event Event type: OK 10/19/2017 7:17:11.732 PM (Coding: 16# 34 00 00 05 14 EE FB EF 9B 07 09 F2 39 CB 00 00 38 CB 00 00 00 00 01 DB 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) 4 of 529; Event ID: 16# 02:39CB Error: IO device failure - chd_vfd_6 Outgoing event Event type: OK 10/19/2017 7:17:09.234 PM (Coding: 16# 34 00 00 05 14 EE FB EF 06 1E 51 EB 39 CB 00 00 38 CB 00 00 00 00 02 27 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) 5 of 529; Event ID: 16# 02:39CB Error: IO device failure - ERECTOR BOX Outgoing event Event type: OK 10/19/2017 7:17:08.280 PM (Coding: 16# 34 00 00 05 14 EE FB EE CD 43 02 56 39 CB 00 00 38 CB 00 00 00 00 01 3C 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) 6 of 529; Event ID: 16# 02:39CB Error: IO device failure - IO device not found chd_vfd_5 Incoming event Event type: Error 10/19/2017 7:17:06.246 PM (Coding: 16# 34 01 00 05 14 EE FB EE 54 0A FE 0D 39 CB 00 00 04 B9 00 13 00 00 02 20 00 02 00 00 00 00 00 00 00 00 00 00 81 81 3F 04 00 00 00 00 00 00 00 00 00 00 00 00) 7 of 529; Event ID: 16# 02:39CB Error: IO device failure - Data transfer fault (no frame received) chd_vfd_5 Outgoing event Event type: OK 10/19/2017 7:17:06.245 PM (Coding: 16# 34 00 00 05 14 EE FB EE 53 F6 C5 62 39 CB 00 00 04 BB 00 00 00 00 02 20 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) 8 of 529; Event ID: 16# 02:39CB Error: IO device failure - IO device not found chd_vfd_4 Incoming event Event type: Error 10/19/2017 7:17:06.240 PM (Coding: 16# 34 01 00 05 14 EE FB EE 53 B4 9F 90 39 CB 00 00 04 B9 00 13 00 00 02 19 00 02 00 00 00 00 00 00 00 00 00 00 81 81 3F 04 00 00 00 00 00 00 00 00 00 00 00 00) 9 of 529; Event ID: 16# 02:39CB Error: IO device failure - Data transfer fault (no frame received) chd_vfd_4 Outgoing event Event type: OK 10/19/2017 7:17:06.238 PM (Coding: 16# 34 00 00 05 14 EE FB EE 53 96 3B E0 39 CB 00 00 04 BB 00 00 00 00 02 19 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) 10 of 529; Event ID: 16# 02:39CB Error: IO device failure - IO device not found chd_vfd_3 Incoming event Event type: Error 10/19/2017 7:17:06.235 PM (Coding: 16# 34 01 00 05 14 EE FB EE 53 6A 55 7E 39 CB 00 00 04 B9 00 13 00 00 01 DB 00 02 00 00 00 00 00 00 00 00 00 00 81 81 3F 04 00 00 00 00 00 00 00 00 00 00 00 00) 11 of 529; Event ID: 16# 02:39CB Error: IO device failure - Data transfer fault (no frame received) chd_vfd_3 Outgoing event Event type: OK 10/19/2017 7:17:06.234 PM (Coding: 16# 34 00 00 05 14 EE FB EE 53 57 9B 1E 39 CB 00 00 04 BB 00 00 00 00 01 DB 00 02 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00) AttachmentIO Device Failure-Data Transfer Fault.pdf (146 Downloads) |
Follow us on