5/10/2017 10:43 AM | |
Posts: 7 Rating:
|
Hi there! I have problem with my IO-Link device. Its first time i'm working with iolink and i can't get measurement values from banner ez array field... My problem is that i used S7-PCT tool, all seems to be ok, in PCT i see measurements values, its ok, but in TIA i cant get these values ( maybe i just do it wrong ). In TIA V14 i use "IO_LINK_DEVICE" block, i trigered it, then BUSY tag goes TRUE, after few secs goes FALSE and RD_LEN stay all the time 0, DONE_VALID is FALSE, but i dont get any error... I'm adding some screenshots of program an IODD files of IO-Link device. Attachmentforum.zip (93 Downloads) |
6/13/2017 9:18 AM | |
Joined: 5/8/2017 Last visit: 6/4/2020 Posts: 25 Rating:
|
What kind of device do you have? And where do you look for the values? |
Follow us on