6/6/2023 1:20 PM | |
Joined: 6/5/2023 Last visit: 6/7/2023 Posts: 1 Rating: (0) |
Good afternoon, I started to work with Siemens IOT2050 and followed the setup document placed on forum: SIMATIC_IOT2050_Setting_up_V1.2.1.pdf My devices are: I downloaded sample image v1.1.1 image from here: Siemens IOT downloads page I have tried: |
6/12/2023 3:36 PM | |
Joined: 10/22/2020 Last visit: 10/1/2024 Posts: 169 Rating: (6)
|
Hello, as you are using a Basic FS:04, please use the example image >V1.2.1 as stated here. Are you already able to download V1.3.1? Use a tool like Win32DiskImager to format and write the image to your SD card. Regarding the display port, please make sure you are using an 'active' display port cable, as this is required to recognise a connected monitor during boot. The IOT2050 behaves as programmed - I suggest you try out the pre-installed NodeRED Dashboard functions, for example to provide data via websites. BR |
Follow us on